The CodeWarrior Assembler does not support all GNU extensions. The following table lists the unsupported GNU extensions.
| Extension | Comment |
|---|---|
| Sub-sections (such as .text 2) | The sub-section number is ignored. As a workaround, you can create your own sections with the .section <name> directive. You may have an arbitrary number of text subsections with the names .text1, .text2, etc. |
| Assignment to location counter (such as . = .+4) | As a workaround, you can advance the location counter with .space <expr> |
| Empty expressions defaulting to 0. For example, .byte , equivalent to (.byte 0,0) | There is no workaround for this. You must always supply the arguments. |
| .linkonce directive | The linker automatically detects logically-identical sections, and uses the following factors to determine whether to keep only one or both in the final image:
|
| .octa | 16-byte numbers are not supported directly. As a workaround, you can use consecutive .long directives to build a large number in memory. |
| .quad | 8-byte numbers are not supported directly. As a workaround, you can use consecutive .long directives to build a large number in memory. |