Supported Extensions

The supported GNU extensions, regardless whether you enable GNU assembler compatible syntax are as follows:

The following table lists the supported GNU assembler directives.

Table 1. Supported GNU Assembler Directives
Directive Description Comment
.abort End assembly Supported
.align N,[pad] Align Now accepts optional padding byte
.app-file name Source name Synonym for .file
.balign[wl] N,[pad] Align Align to N (with optional padding value)
.common name,length Common data Reserve space in BSS for global symbol
.def Debugging Accepted but ignored
.desc Debugging Accepted but ignored
.dim Debugging Accepted but ignored
.eject Eject page Accepted but ignored
.endr End repeat refer .irp, .irpc
.endef Debugging Accepted but ignored
.fill N,[size],[val] Repeat data Emit N copies of width `size', value `val'
.hword val.. Half-word Synonym for .short
.ident Tags Accepted but ignored
.ifnotdef name Conditional Synonym for .ifndef
.include name Include file Now accepts single, double or no quotes
.init val.. Word Synonym for .long
.irp name,values Repeat Repeat up to .endr substituting values for name
.irpc name,chars Repeat Repeat up to .endr substituting chars for name
.lcomm name,length Local common Reserve length bytes in bss
.Iflags Ignored Accepted but ignored
.ln lineno Line number Synonym for .line
.list Listing on Switch on listing
.local name Local Macro var Declare name as local to macro
.macro name, args.. Macros Supports GNU syntax, default values, etc
.nolist Listing off Disable listing
.org pos,fill Origin Now allows fill value to be specified
.p2align[wl] N[,pad] Align Align to 2**N, using pad value `pad'
.psize Page size Accepted but ignored
.rept N Repeat Repeat block up to .endr N times
.sbttl Subtitle Accepted but ignored
.scl Debugging Accepted but ignored
.size name,N Set size Set size of name to N
.skip N[,pad] Space Skip N bytes, pad with `pad'
.space N[,pad] Space Skip N bytes, pad with `pad'
.stabd Debugging Accepted but ignored
.stabn Debugging Accepted but ignored
.stabs Debugging Accepted but ignored
.str "string" Contstant string Synonym for .asciz
.string "string" Constant String Synonym for .asciz
.tag Debugging Accepted but ignored
.title Title Accepted but ignored
.type Debugging Ignored in GNU mode
.val Debugging Accepted but ignored
.word Word Synonym for .long