Labels

A label is a symbol that represents an address. The scope of a label depends on whether the label is local or non-local.

The syntax of a label is:

label ::= local_label [ : ] | non-local_label[ : ]

The default settings are that each label ends with a colon (:), a label can begin in any column. However, if you port existing code that does not follow this convention, you should clear the Labels must end with ':' checkbox of the Assembler settings panel. After you clear the checkbox, you may use labels that do not end with colons, but such labels must begin in column 1.

Note: For more information, refer to the Kinetis Assembler General Settings chapter.

In this topic: