List of Assembler Options

The following table lists the command line options you can use with the S12Z Assembler.

Note: Not all tools options have been defined for this release. All descriptions will be available in an upcoming release.
Table 1. Assembler Options
Assembler option
-ArgFile: Specify a file from which additional command line options will be read
-AsmDbg: Emit assembly source file information in debug sections
-Ci: Switch case sensitivity on label names OFF
-CMacAngBrack: Angle brackets for grouping Macro Arguments
-CMacBrackets: Square brackets for macro arguments grouping
-Compat: Compatibility modes
-D: Define Label
-DefLabel: Improves support for data allocation directives
-Env: Set environment variable
-F (-Fh, -F2o, -FA2o, -F2, -FA2): Output file format
-H: Short Help
-I: Include file path
-L: Generate a listing file
-Lasmc: Configure listing file
-Lasms: Configure the address size in the listing file
-Lc: No Macro call in listing file
-Ld: No macro definition in listing file
-Le: No Macro expansion in listing file
-Li: No included file in listing file
-Lic: License information
-LicA: License information about every feature in directory
-LicBorrow: Borrow license feature
-LicWait: Wait until floating license is available from floating License Server
-Ll: Show label statistics
-MacroNest: Configure maximum macro nesting
-MCUasm: Switch compatibility with MCUasm ON
-N: Display notify box
-NoBeep: No beep in case of an error
-NoDebugInfo: No debug information for ELF/DWARF files
-NoEnv: Do not use environment
-ObjN: Object filename specification
-Prod: Specify project file at startup
-Struct: Support for structured types
-V: Prints the Assembler version
-View: Application standard occurrence
-W1: No information messages
-W2: No information and warning messages
-WErrFile: Create "err.log" error file
-Wmsg8x3: Cut filenames in Microsoft format to 8.3
-WmsgCE: RGB color for error messages
-WmsgCF: RGB color for fatal messages
-WmsgCI: RGB color for information messages
-WmsgCU: RGB color for user messages
-WmsgCW: RGB color for warning messages
-WmsgFb (-WmsgFbv, -WmsgFbm): Set message file format for batch mode
-WmsgFi (-WmsgFiv, -WmsgFim): Set message file format for interactive mode
-WmsgFob: Message format for batch mode
-WmsgFoi: Message format for interactive mode
-WmsgFonf: Message format for no file information
-WmsgFonp: Message format for no position information
-WmsgNe: Number of error messages
-WmsgNi: Number of Information messages
-WmsgNu: Disable user messages
-WmsgNw: Number of Warning messages
-WmsgSd: Setting a message to disable
-WmsgSe: Setting a message to Error
-WmsgSi: Setting a message to Information
-WmsgSw: Setting a Message to Warning
-WOutFile: Create error listing file
-WStdout: Write to standard output