-Ld: No macro definition in listing file

Group

Output

Scope

Assembly unit

Syntax
  -Ld
  
  
Arguments

None

Default

None

Description

Instructs the Assembler to generate a listing file but not including any macro definitions. The listing file contains macro invocation and expansion lines as well as expanded include files.

Example
  ASMOPTIONS=-Ld
  
  

In the following example of assembly code, the cpChar macro accepts two parameters. The macro copies the value of the first parameter to the second one.

When the -Ld option is specified, the assembly source code in the following listing along with additional source code ( Listing: Example source code from an include file) from the macro.inc file generates an assembler output listing ( Listing: Example assembler output listing) file:

Listing: Example assembly source code

         XDEF  Start
MyData:  SECTION

char1:   DS.B  1

char2:   DS.B  1

         INCLUDE "macro.inc"

CodeSec: SECTION

Start:

         cpChar char1, char2

         NOP
Listing: Example source code from an include file

cpChar:  MACRO
           LD D0,  \1

           ST D0,  \2

         ENDM
Listing: Example assembler output listing

 Abs. Rel.   Loc    Obj. code  Source line
 ---- ----   ------ ---------  -----------

    1    1                             XDEF  Start

    2    2                     MyData:  SECTION

    3    3   000000            char1:   DS.B  1

    4    4   000001            char2:   DS.B  1

    5    5                              INCLUDE "macro.inc"

    6    1i                    cpChar:  MACRO

   10    6                     CodeSec: SECTION

   11    7                     Start:

   12    8                              cpChar char1, char2

   13    2m  000000 xx xxxx   +         LD D0, char1

   14    3m  000003 xx xxxx   +         ST D0, char2

   15    9   000006 01                  NOP

The Assembler stores that content of included files in the listing file. The Assembler also stores macro invocation and expansion in the listing file.

The listing file does not contain the source code from the macro definition.

For a detailed description of the listing file, see the Assembler Listing File chapter.

See also

Assembler options: