Output
Assembly unit
-Li
None
None
Switches on the generation of the listing file, but include files are not expanded in the listing file. The listing file contains macro definition, invocation, and expansion lines.
ASMOPTIONS=-Li
In the following example of assembly code, the cpChar macro accepts two parameters. The macro copies the value of the first parameter to the second one.
When -Li option is specified, the assembly source code in the following listing along with additional source code ( Listing: Example source code in an include file) from the macro.inc file generates the following output in the assembly listing file:
XDEF Start MyData: SECTION char1: DS.B 1 char2: DS.B 1 INCLUDE "macro.inc" CodeSec: SECTION Start: cpChar char1, char2 NOP
cpChar: MACRO LD D0, \1 ST D0, \2 ENDM
Abs. Rel. Loc Obj. code Source line ---- ---- ------ --------- ----------- 1 1 XDEF Start 2 2 MyData: SECTION 3 3 000000 char1: DS.B 1 4 4 000001 char2: DS.B 1 5 5 INCLUDE "macro.inc" 10 6 CodeSec: SECTION 11 7 Start: 12 8 cpChar char1, char2 13 2m 000000 xx xxxx + LD D0, char1 14 3m 000003 xx xxxx + ST D0, char2 15 9 000006 01 NOP
The Assembler stores the macro definition, invocation, and expansion in the listing file.
The Assembler does not store the content of included files in the listing file.
For a detailed description of the listing file, see the Assembler Listing File chapter.
Assembler options: