The Environment tab of the Configuration dialog box is used to configure the environment. The following image displays the Environment tab.
The content of the dialog box is read from the actual project file out of the [ Environment Variables] section.
The following table lists the available variables:
| Path | Environment variable |
|---|---|
| General | GENPATH |
| Object | OBJPATH |
| Text | TEXTPATH |
| Absolute | ABSPATH |
| Header File | LIBPATH |
Various Environment Variables: other variables not covered in the above table.
The following buttons are available for the Configuration dialog box:
Note that the variables are written to the project file only if you press the Save button (or using File > Save Configuration or Ctrl + S). In addition, it can be specified in the Save Configuration dialog box if the environment is written to the project file or not.