Use this dialog box to set or reset assembler options. The following image displays the S12Z Assembler Option Settings dialog box.
The options available are arranged into different groups, and a sheet is available for each of these groups. The content of the list box depends on the selected sheet:
| Group | Description |
|---|---|
| Output | Lists options related to the output files generation (which kind of file should be generated). |
| Input | Lists options related to the input files. |
| Language | Lists options related to the programming language (ANSI-C, C++, etc.) |
| Host | Lists options related to the host. |
| Code Generation | Lists options related to code generation (memory models, etc.) |
| Messages | Lists options controlling the generation of error messages. |
| Various | Lists various additional options, such as options used for compatibility. |
An assembler option is set when the check box in front of it is checked. To obtain more detailed information about a specific option, select it and press the F1key or the Help button. To select an option, click once on the option text. The option text is then displayed inverted.
When the dialog box is opened and no option is selected, pressing the F1key or the Help button shows the help about this dialog box.
The available options are listed in the Assembler Options chapter.