The following listing shows another assembly code file module for this project.
XDEF entry INCLUDE "Test1.inc" CodeSec: SECTION entry: RSP LD D0, #$7 JSR AddSource BRA entry
The application's *.prm file should list both object files building the application. When a section is present in the different object files, the object file sections are concatenated into a single absolute file section. The different object file sections are concatenated in the order the object files are specified in the *.prm file.