XDEF [.<size>] <label>[,<label>]...
where <size> = B(direct), W (default), L or S or T
GLOBAL, PUBLIC
This directive specifies labels defined in the current module that are to be passed to the linker as labels that can be referenced by other modules linked to the current module.
The number of symbols enumerated in an XDEF directive is only limited by the memory available at assembly time.
The S and T size designators are only available for S12Z, and result in marking the symbol as short or tiny.
See the following listing for the case where the XDEF assembler directive can specify symbols that can be used by other modules.
XDEF Count, main ;; variable Count can be referenced in other modules, ;; same for label main. Note that Linker & Assembler ;; are case-sensitive, i.e., Count != count. Count: DS.W 2 code: SECTION main: DC.B 1