[<label>:] DC [.<size>] <expression> [, <expression>]...
where <size> = B (default), W, or L.
DCW (= 2 byte DCs), DCL (= 4 byte DCs),
FCB (= DC.B), FDB (= 2 byte DCs),
FQB (= 4 byte DCs)
The DC directive defines constants in memory. It can have one or more <expression> operands, which are separated by commas. The <expression> can contain an actual value (binary, octal, decimal, hexadecimal, or ASCII). Alternatively, the <expression> can be a symbol or expression that can be evaluated by the Assembler as an absolute or simple relocatable expression. One memory block is allocated and initialized for each expression.
The following rules apply to size specifications for DC directives:
000000 4142 4344 Label: DC.B "ABCDE" 000004 45 000005 0A0A 010A DC.B %1010, @12, 1,$A
000000 0041 4243 Label: DC.W "ABCDE" 000004 4445 000006 000A 000A DC.W %1010, @12, 1, $A 00000A 0001 000A 00000E xxxx DC.W Label
000000 0000 0041 Label: DC.L "ABCDE" 000004 4243 4445 000008 0000 000A DC.L %1010, @12, 1, $A 00000C 0000 000A 000010 0000 0001 000014 0000 000A 000018 xxxx xxxx DC.L Label
If the value in an operand expression exceeds the size of the operand, the assembler truncates the value and generates a warning message.
Assembler directives: