Reserved symbols

Reserved symbols cannot be used for user-defined symbols.

Register names are reserved identifiers.

For the S12Z processor the reserved identifiers are listed in the following listing:

Listing: Reserved identifiers for an HCS12Z derivative

A, CCR, H, X, SP

The keywords LOW and HIGH are also reserved identifiers. They are used to refer to the low byte and the high byte of a memory location.