Use Drag and Drop

A filename can be dragged from an external software (for example the File Manager/ Explorer) and dropped into the assembler window. The dropped file will be assembled when the mouse button is released in the assembler window. If a file being dragged has the *.ini extension, it is considered to be a configuration and it is immediately loaded and not assembled. To assemble a source file with the *.ini extension, use one of the other methods.