S12Z Assembler > Language

Use this panel to specify code- and symbol-generation options for the S12Z assembler.

The following table lists and describes the language options for S12Z assembler.

Table 1. Tool Settings - S12Z Assembler > Language Options
Option Description
Angle Brackets for Macro Arguments Grouping For description, refer to the topic -CMacAngBrack: Angle brackets for grouping Macro Arguments.
Square Braces for Macro Arguments Grouping For description, refer to the topic -CMacBrackets: Square brackets for macro arguments grouping.
Maximum Macro Nesting For description, refer to the topic -MacroNest: Configure maximum macro nesting.