Use this panel to specify file search paths and any additional include files the S12Z Assembler should use. You can specify multiple search paths and the order in which you want to perform the search.
The following table lists and describes the input options for S12Z assembler.
| Option | Description |
|---|---|
| Case Insensitivity on Label Name | For description, refer to the topic -Ci: Switch case sensitivity on label names OFF. |
| Define Label (use spaces to separate labels) | For description, refer to the topic -D: Define Label. |
| Support for Structured Types | For description, refer to the topic -Struct: Support for structured types. |
| Include File Search Path | For description, refer to the topic -I: Include file path. |