S12Z Assembler > Host

Use this panel to specify the host settings of the S12Z assembler.

The following table lists and describes the memory model options for S12Z assembler.

Table 1. Tool Settings - S12Z Assembler > Host Options
Option Description
Borrow License Feature For description, refer to the topic -LicBorrow: Borrow license feature.
Wait Until a License is Available from Floating License Server For description, refer to the topic -LicWait: Wait until floating license is available from floating License Server.
Application Standard Occurrence For description, refer to the topic -View: Application standard occurrence.
Set Environment Variable For description, refer to the topic -Env: Set environment variable.