S12Z Assembler

Use this panel to specify the command, options, and expert settings for the build tool assembler.

The following table lists and describes the assembler options for S12Z architectures.

Table 1. Tool Settings - Assembler Options
Option Description
Command Shows the location of the assembler executable file. You can specify additional command line options for the assembler; type in custom flags that are not otherwise available in the UI.
All options Shows the actual command line the assembler will be called with.

Expert Settings

Command line pattern

Shows the command line pattern; default is ${COMMAND} ${FLAGS} ${OUTPUT_FLAG}${OUTPUT_PREFIX}${OUTPUT} ${INPUTS}