A project directory contains all of the environment files that you need to configure your development environment.
There are three methods of designing a project.
Start from scratch, make your project configuration (*.ini) and layout files for use with the Build Tools,
Use CodeWarrior IDE to coordinate and manage the entire project, or
Begin project construction with CodeWarrior IDE and use the standalone build tools to complete the project.
Note:
The Build Tools (including Assembler, Compiler, Linker, Simulator/ Debugger, and others) are a part of the CodeWarrior Suite and are located in the
prog folder in the CodeWarrior installation. The default location this folder is: