Controls how strictly the compiler checks headers for standard C library functions.
#pragma strictheaderchecking on | off | reset
The 3.2 version compiler recognizes standard C library functions. If the correct prototype is used, and, in C++, if the function appears in the " std" or root namespace, the compiler recognizes the function, and is able to optimize calls to it based on its documented effects.
When this #pragma is on (default), in addition to having the correct prototype, the declaration must also appear in the proper standard header file (and not in a user header or source file).
This pragma does not correspond to any panel setting. By default, this pragma is on.