Controls the availability of the long long type.
#pragma longlong on | off | reset
When this pragma is enabled and the compiler is translating "C90" source code (ISO/IEC 9899-1990 standard), the compiler recognizes a data type named long long. The long long type holds twice as many bits as the long data type.
This pragma does not correspond to any CodeWarrior IDE panel setting.
By default, this pragma is on for processors that support this type. It is off when generating code for processors that do not support, or cannot turn on the long long type.