Controls the recognition of a non-virtual member function that hides a virtual function in a superclass.
#pragma warn_hidevirtual on | off | reset
If you enable this pragma, the compiler issues a warning message when you declare a non-virtual member function that hides a virtual function in a superclass. One function hides another if it has the same name but a different argument type. The following listing shows an example.
class A { public: virtual void f(int); virtual void g(int); }; class B: public A { public: void f(char); // WARNING: Hides A::f(int) virtual void g(int); // OK: Overrides A::g(int) };
The ISO/IEC 14882-2003 C++ Standard does not require this pragma.