iso_templates

Controls whether or not to use the new parser supported by the CodeWarrior 2.5 C++ compiler and issue warning messages for missing typenames.

Syntax
  #pragma iso_templates on | off | reset
  
  
Remarks

This pragma combines the functionality of pragmas parse_func_templ, parse_mfunc_templ and warn_no_typename.

This pragma ensures that your C++ source code is compiled using the newest version of the parser, which is stricter than earlier versions. The compiler issues a warning message if a typename required by the C++ standard is missing but can still be determined by the compiler based on the context of the surrounding C++ syntax.

By default, this pragma is on.