__optlevelx

Optimization level exported as a predefined macro.

Syntax
  __optlevel0
  
  
  __optlevel1
  
  
  __optlevel2
  
  
  __optlevel3
  
  
  __optlevel4
  
  
Remarks

Using these macros, user can conditionally compile code for a particular optimization level. The following table lists the level of optimization provided by the __optlevelx macro.

Table 1. Optimization Levels
Macro Optimization Level
__optlevel0 O0
__optlevel1 O1
__optlevel2 O2
__optlevel3 O3
__optlevel4 O4
Example

The listing below shows an example of __optlevelx macro usage.

Listing: Example usage of __optlevel macro

int main()
{

#if __optlevel0

... // This code compiles only if this code compiled with Optimization

level 0

#elif __optlevel1

... // This code compiles only if this code compiled with Optimization

level 1

#elif __optlevel2

... // This code compiles only if this code compiled with Optimization

level 2

#elif __optlevel3

... // This code compiles only if this code compiled with Optimization

level 3

#elif __optlevel4

... // This code compiles only if this code compiled with Optimization

level 4

#endif

}