Because the compiler treats all files that compose a program as if they were a single, large source file, you must make sure all non-static declarations for variables or functions with the same name are identical. The following listing for an example of declarations that prevent the compiler from applying program-level analysis.
/* file1.c */ extern int i; extern int f(); int main(void) { return i + f(); } /* file2.c */ short i; /* Conflict with variable i in file1.c. */ extern void f(); /* Conflict with function f() in file1.c */
The following listing fixes this problem by renaming the conflicting symbols.
/* file1.c */ extern int i1; extern int f1(); int main(void) { return i1 + f1(); } /* file2.c */ short i2; extern void f2();