The compiler offers several methods to specify which functions are eligible for inlining.
To specify that a function is eligible to be inlined, precede its definition with the inline, __inline__, or __inline keyword. To allow these keywords in C source code, turn off ANSI Keywords Only in the CodeWarrior IDE's C/C++ Language settings panel or turn off the only_std_keywords pragma in your source code.
To verify that an eligible function has been inlined or not, use the Non-Inlined Functions option in the IDE's C/C++ Warnings panel or the warn_notinlined pragma. The following listing shows an example.
#pragma only_std_keywords off inline int attempt_to_inline(void) { return 10; }
To specify that a function must never be inlined, follow its definition's specifier with __attribute__((never_inline)). The following listing shows an example.
int never_inline(void) __attribute__((never_inline)) { return 20; }
To specify that no functions in a file may be inlined, including those that are defined with the inline, __inline__, or __inline keywords, use the dont_inline pragma. The following listing shows an example.
#pragma dont_inline on /* Will not be inlined. */ inline int attempt_to_inline(void) { return 10; } /* Will not be inlined. */ int never_inline(void) __attribute__((never_inline)) { return 20; } #pragma dont_inline off /* Will be inlined, if possible. */ inline int also_attempt_to_inline(void) { return 10; }
The kind of functions that never inlined are:
The compiler will not inline these functions, even if they are defined with the inline, __inline__, or __inline keywords.
The following functions also should never be inlined:
It can inline such functions if the class has a trivial empty constructor as in this case:
struct X { int n; X(int a) { n = a; } ~X() {} }; inline X f(X x) { return X(x.n + 1); } int main() { return f(X(1)).n; }
This does not depend on "ISO C++ templates".