Extensions to the Preprocessor

When ANSI strictness is off, the C compiler allows a # to prefix an item that is not a macro argument. It also allows an identifier after an #endif directive. Listing: Using # in Macro Definitions and Listing: Identifiers After #endif show examples.

Listing: Using # in Macro Definitions

#define add1(x) #x #1

    /* OK, if ANSI_strict is disabled,

       but probably not what you wanted:

       add1(abc) creates "abc"#1 

     */

#define add2(x) #x "2"

    /* Always OK: add2(abc) creates "abc2". */
Listing: Identifiers After #endif

#ifdef __CWCC__

  /* . . . */

#endif __CWCC__ /* OK if ANSI_strict is disabled. */

#ifdef __CWCC__

  /* . . . */

#endif /*__CWCC__*/ /* Always OK. */