-defaults

Controls whether the compiler uses additional environment variables to provide default settings.

Syntax
  -defaults
  
  
  -nodefaults
  
  
Remarks

This option is global. To tell the command-line compiler to use the same set of default settings as the CodeWarrior IDE, use -defaults. For example, in the IDE, all access paths and libraries are explicit. defaults is the default setting.

Use -nodefaults to disable the use of additional environment variables.