-instmgr

Controls whether the instance manager for templates is active.

Syntax
  -inst[mgr] keyword [,...]
  
  

The options for keyword are:

off

Turns off the C++ instance manager. This is the default.

on

Turns on the C++ instance manager.

file=path

Specify the path to the database used for the C++ instance manager. Unless specified the default database is cwinst.db.

Remarks

This command is global. The default setting is off.