Use environment variables on the host system to specify to the CodeWarrior command line tools where to find CodeWarrior files for compiling and linking. The following table describes these environment variables.
| This environment variable... | specifies this information |
|---|---|
| MWCIncludes | Directories on the host system for system header files for the CodeWarrior compiler. |
| MWLibraries | Directories on the host system for system libraries for the CodeWarrior linker. MWLibraries are used with the automatic library selection linker flag, -lavender. |
| CWFolder | CodeWarrior installation path on the host system. |
A system header file is a header file that is enclosed with the < and > characters in include directives. For example,
#include <stdlib.h> /* stdlib.h system header. */
Typically, you define the MWCIncludes and MWLibraries environment variables to refer to the header files and libraries in the subdirectories of your CodeWarrior software.
To specify more than one directory for the MWCIncludes and MWLibraries variables, use the conventional separator for your host operating system command-line shell.
rem Use ; to separate directory paths set CWFolder=C:\Freescale\CodeWarrior set MWCIncludes=%CWFolder%\MCU\ARM_EABI_Support\ewl\EWL_C\Include set MWCIncludes=%MWCIncludes%;%CWFolder%\MCU\ARM_EABI_Support\ewl\EWL_C++\Include set MWCIncludes=%MWCIncludes%;%CWFolder%\MCU\ARM_EABI_Support\ewl\EWL_C\Include\sys set MWLibraries=%CWFolder%\MCU\ARM_EABI_Support\ewl\lib