Using the CodeWarrior MCU Wizard to Create a Project

Use the CodeWarrior MCU wizard to create and manage your project. Follow the steps in this section to create a project and generate the basic project files.

Using the Wizard provides instructions for creating and configuring a basic CodeWarrior project that uses C source code to build an application. Through the wizard, the Eclipse IDE manages the integrated Build Tools.