The following sections describe the settings panels that configure the build tool options. These panels are the part of the project's build properties settings, which are managed in the Properties window. To access these panels, proceed as follows:
A Properties for <project> dialog box appears.
The settings for the build tools appear. If not, click on the Tool Settings tab.
Based on the build tool you selected while creating the project you may have: