This chapter covers the primary method to create a project with the CodeWarrior Development Studio for Microcontrollers, Version 10.x.
Note: Information on the other Build Tools can be found in User Guides included with the CodeWarrior Suite and are located in the Help folder for the CodeWarrior installation. The default location of this folder is C:\Freescale\CW MCU v10.x\MCU\Help
The topics covered here are as follows: