text_encoding

Identifies the character encoding of source files.

Syntax
  #pragma text_encoding ( "name" | unknown | reset [, global] )   
Parameters

name

The IANA or MIME encoding name or an OS-specific string that identifies the text encoding. The compiler recognizes these names and maps them to its internal decoders:

system US-ASCII ASCII ANSI_X3.4-1968

ANSI_X3.4-1968 ANSI_X3.4 UTF-8 UTF8 ISO-2022-JP

CSISO2022JP ISO2022JP CSSHIFTJIS SHIFT-JIS

SHIFT_JIS SJIS EUC-JP EUCJP UCS-2 UCS-2BE

UCS-2LE UCS2 UCS2BE UCS2LE UTF-16 UTF-16BE

UTF-16LE UTF16 UTF16BE UTF16LE UCS-4 UCS-4BE

UCS-4LE UCS4 UCS4BE UCS4LE 10646-1:1993

ISO-10646-1 ISO-10646 unicode

global

Tells the compiler that the current and all subsequent files use the same text encoding. By default, text encoding is effective only to the end of the file.

Remarks

By default, #pragmatext_encoding is only effective through the end of file. To affect the default text encoding assumed for the current and all subsequent files, supply the "global" modifier.