mpwc_relax

Controls the compatibility of the char* and unsigned char* types.

Syntax
  #pragma mpwc_relax on | off | reset   
Remarks

If you enable this pragma, the compiler treats char* and unsigned char* as the same type. Use this setting to compile source code written before the ISO C standards. Old source code frequently uses these types interchangeably.

This setting has no effect on C++ source code.

Note: Turning this option on may prevent the compiler from detecting some programming errors. We recommend not turning on this option.

The following listing shows how to use this pragma to relax function pointer checking.

Listing: Relaxing function pointer checking
#pragma mpwc_relax on 
extern void f(char *); 
/* Normally an error, but allowed. */ 
extern void(*fp1)(void *) = &f; 
/* Normally an error, but allowed. */ 
extern void(*fp2)(unsigned char *) = &f; 

This pragma does not correspond to any panel setting. By default, this pragma is disabled.