old_pods

Permits non-standard handling of classes, structs, and unions containing pointer-to-pointer members

Syntax
  #pragma old_pods on | off | reset   
Remarks

According to the ISO/IEC 14882:2003 C++ Standard, classes/structs/unions that contain pointer-to-pointer members are now considered to be plain old data (POD) types.

This pragma can be used to get the old behavior.