Strength Reduction

Strength reduction attempts to replace slower multiplication operations with faster addition operations. This optimization improves execution speed but increases code size.

The following table explains how to control the optimization for strength reduction.

Table 1. Controlling strength reduction
Turn control this option from here... use this setting
CodeWarrior IDE Choose Level 3 or Level 4 in the Optimization Level settings panel.
source code #pragma opt_strength_reduction on | off | reset
command line -opt [no]strength

For example, in the following listing, the assignment to elements of the vec array use a multiplication operation that refers to the for loop's counter variable, i.

Listing: Before strength reduction
void func_from(int* vec, int max, int fac)

{

    int i;

    for (i = 0; i < max; ++i)

    {

        vec[i] = fac * i;

    }

}

In the code listed below, the compiler has replaced the multiplication operation with a hidden variable that is increased by an equivalent addition operation. Processors execute addition operations faster than multiplication operations.

Listing: After strength reduction
void func_to(int* vec, int max, int fac)

{

    int i;

    int strength_red;

    hidden_strength_red = 0;

    for (i = 0; i < max; ++i)

    {

        vec[i] = hidden_strength_red;

        hidden_strength_red = hidden_strength_red + i;

    }

}