Allows changing the format for float (by default IEEE32).
-float_size 4 | 8
The arguments are as follows:
4 : IEEE32
8 : IEEE64
4
__FLOAT_IS_IEEE32__
__FLOAT_IS_IEEE64__
For integrity and compliance to ANSI, the following must hold:
sizeof(float) <= sizeof(double)
For more information, refer to the topic Data Types.