Getting Help

To show short descriptions of a tool's options, type this command at the command line:

  tool -help   

where tool is the name of the CodeWarrior build tool.

To show only a few lines of help information at a time, pipe the tool's output to a pager program. For example,

  tool -help | more   

will use the more pager program to display the help information.

Enter the following command in a Command Prompt window to see a list of specifications that describe how options are formatted:

  tool -help usage   

where tool is the name of the CodeWarrior build tool.