Scalar Types

Type char is by default unsigned (that is, char is the same as unsigned char). The other scalar types are all signed by default (for example, int is the same as signed int).

The following table specifies the possible formats for each of the supported scalar types:

Table 1. Scalar Types
Type Default Format Default Value Range Alternative Formats (flexible type configuration)
Min Max
char (unsigned) 8-bit 0 255 8-, 16-, & 32-bit
signed char 8-bit -128 127 8-, 16-, & 32-bit
unsigned char 8-bit 0 255 8-, 16-, & 32-bit
signed short 16-bit -32,768 32,767 8-, 16-, & 32-bit
unsigned short 16-bit 0 65,535 8-, 16-, & 32-bit
enum (unsigned) 16-bit 0 65,535 8-, 16-, & 32-bit
signed int 16-bit -32,768 32,767 8-, 16-, & 32-bit
unsigned int 16-bit 0 65,535 8-, 16-, & 32-bit
signed long 32-bit -2,147,483,648 2,147,483,647 8-, 16-, & 32-bit
unsigned long 32-bit 0 4,294,967,295 8-, 16-, & 32-bit
signed long long 32-bit -2,147,483,648 2,147,483,647 8-, 16-, & 32-bit
unsigned long long 32-bit 0 4,294,967,295 8-, 16-, & 32-bit
For more information, refer to the following topics: