S12Z Compiler > Language

Use this panel to specify the language settings for S12Z compiler.

The following table lists and describes the Language options for S12Z compiler.

Table 1. Tool Settings - S12Z Compiler > Language Options
Option Description
Require Function Prototypes Check to enforce the requirement of function prototypes. The compiler generates an error message if you define a previously referenced function that does not have a prototype. If you define the function before it is referenced but do not give it a prototype, this setting causes the compiler to issue a warning message.
Enable C++ 'bool' type, 'true' and 'false' Constants Check to enable the C++ compiler to recognize the bool type and its true and false values specified in the ISO/IEC 14882-2003 C++ standard.
ISO C++ Template Parser Check to follow the ISO/IEC 14882-2003 standard for C++ to translate templates, enforcing more careful use of the typename and template keywords. The compiler also follows stricter rules for resolving names during declaration and instantiation.
Use Instance Manager Check to reduce compile time by generating any instance of a C++ template (or noninlined inline) function only once.
Force C++ Compilation Check to enable the forced C++ compilation.
Enable GCC Extensions Check to recognize language features of the GNU Compiler Collection (GCC) C compiler that are supported by CodeWarrior compilers; is equivalent to pragma gcc_extensions and the command-line option -gcc_extensions.
Enable C99 Extensions Check to recognize ISO/IEC 9899-1999 ("C99") language features; is equivalent to pragma c99 and the command-line option -dialect c99.
Enable C++ Exceptions Check to generate executable code for C++ exceptions; is equivalent to pragma exceptions and the command-line option -cpp_exceptions.
Enable RTTI Check to allow the use of the C++ runtime type information (RTTI) capabilities, including the dynamic_cast and typeid operators; is equivalent to pragma RTTI and the command-line option -RTTI.
Enable wchar_t Support Check to enable C++ compiler recognize the wchar_t data type specified in the ISO/IEC 14882-2003 C++ standard; is equivalent to pragma wchar_type and the command-line option -wchar_t.
ANSI Strict Check to enable C compiler operate in strict ANSI mode. In this mode, the compiler strictly applies the rules of the ANSI/ISO specification to all input files. This setting is equivalent to specifying the - ansi command-line option. The compiler issues a warning for each ANSI/ISO extension it finds.
ANSI Keywords Only Check to generate an error message for all non-standard keywords (ISO/IEC 9899-1990 C, §6.4.1). If you must write source code that strictly adheres to the ISO standard, enable this setting; is equivalent to pragma only_std_keywords and the command-line option -stdkeywords.
Expand Trigraphs Check to recognize trigraph sequences (ISO/ IEC 9899-1990 C, §5.2.1.1); is equivalent to pragma trigraphs and the commandline option -trigraphs.
Legacy for-scoping Check to generate an error message when the compiler encounters a variable scope usage that the ISO/IEC 14882-2003 C++ standard disallows, but is allowed in the C++ language specified in The Annotated C++ Reference Manual ("ARM"); is equivalent to pragma ARM_scoping and the command-line option -for_scoping.
Enum Always Int Check to use signed integers to represent enumerated constants and is equivalent to pragma enumsalwaysint and the command-line option -enum.
Use Unsigned Chars Check to treat char declarations as unsigned char declarations and is equivalent to pragma unsigned_char and the command-line option -char unsigned.
Reuse Strings Check to store only one copy of identical string literals and is equivalent to opposite of the pragma dont_reuse_strings and the command-line option -string reuse.
Pool Strings Check to collect all string constants into a single data section in the object code it generates and is equivalent to pragma pool_strings and the command-line option -strings pool.