S12Z Compiler > General

Use this panel to specify the general compiler behavior.

The following table lists and describes the general compiler options for S12Z architecture.

Table 1. Tool Settings - Linker > General Options
Option Description
Generate Debug Information This option allows the compiler to generate the debug information. By default, this checkbox is checked.
Other Flags Specify additional command line options for the linker; type in custom flags that are not otherwise available in the UI.