The following sections describe the settings panels that configure the build tool options. These panels are part of the project's build properties settings, which are managed in the Properties for <project> dialog box. To access these panels, proceed as follows:
A Properties for <project> dialog box appears.
The settings for the build tools are displayed in the right panel of the Properties for <project> dialog box. If not, click on the Tool Settings tab.
The options are grouped by tool, such as S12Z Burner options, S12Z Linker options, S12Z Compiler options, and so on. Scroll down the list, and click on the option whose settings you wish to examine and modify.
The following table lists the build properties specific to developing software for S12Z.
The properties that you specify in these panels, apply to the selected build tool on the Tool Settings page of the Properties for <project> dialog box.