[DISABLED]
The compiler generated an especially slow code pattern. The actual limit is CPU dependent.
- See if the C code can be rewritten so that faster code is generated.
- See if powers of two can be used for dividends.
- Try to use unsigned types.
- Try to use smaller types.