[DISABLE]
A variable was allocated differently because of a pragma INTO_ROM or a pragma FAR.
#pragma INTO_ROM
const int i;
Be careful with the pragmas INTO_ROM and pragma FAR. They are only valid for one single variable. In the following code the pragma INTO_ROM puts var_rom into the rom, but var_ram not.
#pragma INTO_ROM
const int var_rom, var_ram;
Note that pragma INTO_ROM is only for the HIWARE Object file format.