If the Simulator or Debugger cannot be launched, check the settings in the project's launch configuration. For more information on launch configurations and their settings, refer to the Microcontrollers V10.x Targeting Manual.
If a file cannot be added to the project, its file extension may not be available in the File Types panel. To resolve the issue, add the file's extension to the list in the File Types panel. To access the File Types panel, proceed as follows:
The Properties for < project > window appears.
The changes are saved and the properties dialog box closes.