MESSAGES
None
-WmsgNu[={a|b|c|d}]
a: Disable messages about include files
b: Disable messages about reading files
c: Disable messages about generated files
d: Disable messages about processing statistics
e: Disable informal messages
t: Display type of messages
None
None
None
The application produces messages that are not in the following normal message categories: WARNING, INFORMATION, ERROR, or FATAL. This option disables messages that are not in the normal message category by reducing the amount of messages, and simplifying the error parsing of other tools.
a: Disables the application from generating information about all included files.
b: Disables messages about reading files (e.g., the files used as input) are disabled.
c: Disables messages informing about generated files.
d: Disables information about statistics (e.g., code size, RAM, or ROM usage).
e: Disables informal messages (e.g., memory model, floating point format).
t: Displays type of messages.
-WmsgNu=c