-WmsgNe: Maximum Number of Error Messages

Group

MESSAGES

Scope

Compilation Unit

Syntax
  -WmsgNe<number> 
  
Arguments

<number>: Maximum number of error messages

Default

50

Defines

None

Pragmas

None

Description

This option sets the number of error messages that are to be displayed while the Compiler is processing.

Note: Subsequent error messages which depend upon a previous error message may not process correctly.
Example

-WmsgNe2

Stops compilation after two error messages

See also

-WmsgNi: Maximum Number of Information Messages

-WmsgNw: Maximum Number of Warning Messages