OUTPUT
Function
-Lasmc[={a|c|i|s|h|p|e|v|y}]
a: Do not write the address
c: Do not write the code
i: Do not write the instruction
s: Do not write the source code
h: Do not write the function header
p: Do not write the source prolog
e: Do not write the source epilog
v: Do not write the compiler version
y: Do not write cycle information
All printed together with the source
None
None
The -Lasmc option configures the output format of the listing file generated with the -Lasm: Generate Listing File option. The addresses, the hex bytes, and the instructions are selectively switched off.
The format of the listing file has the layout shown in the following listing. The letters in brackets ([]) indicate which suboption may be used to switch it off:
[v] ANSI-C/cC++ Compiler V-5.0.1 [v] [p] 1: [p] 2: void foo(void) { [h] [h] Function: foo [h] Source : C:\Freescale\test.c [h] Options : -Lasm=%n.lst [h] [s] 3: } [a] 0000 [c] 3d [i] RTS [e] 4: [e] 5: // comments [e] 6:
-Lasmc=ac