INPUT
Compilation Unit
-I<path>
<path>: path, terminated by a space or end-of-line
None
None
None
Allows you to set include paths in addition to the LIBPATH, LIBRARYPATH: `include <File>' Path and GENPATH: #include "File" Path environment variables. Paths specified with this option have precedence over includes in the current directory, and paths specified in GENPATH, LIBPATH, and LIBRARYPATH.
-I. -I..\h -I\src\include
This directs the Compiler to search for header files first in the current directory (.), then relative from the current directory in '..\h', and then in '\src\include'. If the file is not found, the search continues with GENPATH, LIBPATH, and LIBRARYPATH for header files in double quotes ( #include"headerfile.h"), and with LIBPATH and LIBRARYPATH for header files in angular brackets ( #include <stdio.h>).