CODE GENERATION
Function
-BfaGapLimitBits<number>
<number>: positive number specifying the maximum number of bits for a gap
1
None
None
The bitfield allocation tries to avoid crossing a byte boundary whenever possible. To achieve optimized accesses, the compiler may insert some padding or gap bits to reach this. This option enables you to affect the maximum number of gap bits allowed.
In the example in the following listing, assume that you have specified a 3-bit maximum gap, i.e., -BfaGapLimitBits3.
struct { unsigned char a: 7; unsigned char b: 5; unsigned char c: 4; } B;
The compiler allocates struct B with 3 bytes. First, the compiler allocates the 7 bits of a. Then the compiler tries to allocate the 5 bits of b, but this would cross a byte boundary. Because the gap of 1 bit is smaller than the specified gap of 3 bits, b is allocated in the next byte. Then the allocation starts for c. After the allocation of b there are 3 bits left. Because the gap is 3 bits, c is allocated in the next byte. If the maximum gap size were specified to zero, all 16 bits of B would be allocated in two bytes. Since the gap limit is set to 3, and the gap required for allocating c in the next byte is also 3, the compiler will use a 16-bit word as the allocation unit. Both b and c will be allocated within this word.
Assuming we initialize an instance of B as below:
B s = {2, 7, 5},
we get the following memory layouts:
-BfaGapLimitBits1 : 53 82
-BfaGapLimitBits3 : 02 00 A7
-BfaGapLimitBits4 : 02 07 05 m
The following listing specifies a maximum size of two bits for a gap.
-BfaGapLimitBits2